DIN.LCMD1 to DIN.LCMD4
Description
DIN.LCMDx sets the string of commands to be used in the digital input mode command buffer. Digital input mode 9-Command buffer can execute four different sets of command buffers.
Each set of command buffers contains two buffers:
- High buffer: Executes upon a rising edge
A rising edge is the transition of a digital signal from low to high. It is also called positive edge of a digital input.
- Low buffer: Executes upon a falling edge of a digital input.
DIN.LCMDx sets the string for the four "low" buffers, depending on x.
Example
Set the command buffer mode to digital input 1:
DIN1.MODE 9
Set the first sets of buffers to digital input 1:
DIN1.PARAM 1
Set the command DRV.OPMODE 0 to the "low buffer":
DIN.LCMD1 DRV.OPMODE 0
Now, upon a falling edge in digital input 1, the drive mode is 0.
General Information
|
Type |
NV parameter |
|
Units |
N/A |
|
Range |
A string of up to 128 characters |
|
Default Value |
Empty |
|
Data Type |
String |
|
Start Version |
M_01-02-08-000 |
Related Topics
Command Buffer
DIN1.MODE TO DIN7.MODE, DIN1.PARAM TO DIN7.PARAM, DIN.HCMD1 TO DIN.HCMD4
|
Copyright © 2018 Kollmorgen |
|