DIN.STATES

Description

DIN.STATES reads the states of the digital inputs. The leftmost bit represents digital input 1 (DIN1) and the rightmost bit represents digital input 7 (DIN7).

General Information

Type

R/O Parameter

Units

N/A

Range

0000000 to 1111111

Default Value

N/A

Data Type

String

Start Version

M_01-00-00-000

Related Topics

Digital Inputs and Outputs

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen