DOUT.STATES

Description

DOUT.STATES reads the states of the digital output(s). The leftmost bit represents DOUT1 and the rightmost bit represents DOUT2.

General Information

Type

R/O Parameter

Units

N/A

Range

0 to 11

Default Value

N/A

Data Type

String

BASIC: Integer

Start Version

M_01-00-00-000

Related Topics

Digital Outputs

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen