DOUT1.MODE to DOUT2.MODE
|
General Information |
|
|---|---|
|
Type |
NV Parameter |
|
Description |
|
|
Units |
N/A |
|
Range |
0 to 22 |
|
Default Value |
0 |
|
Data Type |
Integer |
|
Start Version |
M_01-04-02-000 |
| AKD BASIC Information | |
|---|---|
| Range | 0, 8, 10, 11, 15 |
| AKD-C Information | |
|---|---|
| Range | 0, 1, 7, 11, 16 |
| AKD EtherNet/IP Information | |
|---|---|
| Range | 0 to 2 |
|
Index/Subindex |
Parameter |
Object Start Version |
|
|---|---|---|---|
|
35AFh/0 |
DOUT1.MODE |
M_01-00-00-000 |
|
|
35B2h/0 |
DOUT2.MODE |
Description
DOUTx.MODE sets the functionality of the digital output(s). The table below summarizes the digital output modes; for detailed descriptions of each mode, see Digital Inputs and Outputs.
|
DOUTx.MODE |
Description |
|---|---|
|
User (default = 0) |
|
|
Mains ready |
|
|
Software limit switch reached |
|
|
Move complete |
|
|
In position |
|
|
Position greater than x |
|
|
Position less than x |
|
|
Drive produced warning |
|
|
Drive enabled |
|
|
Reserved |
|
|
Motor brake |
|
|
Drive produced fault |
|
|
Absolute velocity greater than x |
|
|
Absolute velocity less than x |
|
|
PLS.STATE bits or connected |
|
| 16 | Description Command buffer Active |
| 17 | Mt in Position |
| 20 | Controlled Stop Active |
| 21 | Immediate Fault Disable |
| 22 | In Rush Relay State |
Related Topics
|
Copyright © 2018 Kollmorgen |
|