DRV.BOOTTIME
Description
DRV.BOOTTIME returns the time that the current session started running.This time includes total amount of time from all previous sessions.
This keyword can be used with DRV.RUNTIME to determine the length of time the drive has been running since it was last power cycled.
Session Time = DRV.RUNTIME – DRV.BOOTTIME
General Information
|
Type |
R/O |
|
Units |
Days:Hours:Minutes:Seconds |
|
Range |
N/A |
|
Default Value |
N/A |
|
Data Type |
String |
|
Start Version |
M_01-06-05-000 |
Related Topics
|
Copyright © 2018 Kollmorgen |
|