DRV.CMDDELAY

Description

This parameter is used when drive commands are used in a script and a delay is needed between the execution of two consecutive commands. DRV.CMDDELAY creates a delay in the execution of drive commands. In the period of time specified, no commands are executed. This feature is especially useful for command buffers.t

Example

If the script is:

DRV.EN

ILClosed"Instruction list" This is a low-level language and resembles assembly.CMDU 0.1

then DRV.CMDDELAY is used between the two entries to delay execution 5 ms until the drive is enabled:

DRV.EN

DRV.CMDDELAY 5

IL.CMDU 0.1

General Information

Type

Command

Units

ms

Range

0 to 5,000 ms

Default Value

0 ms

Data Type

Float

Start Version

M_01-03-00-000

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen