DRV.DISSOURCESMASK

Description

DRV.DISSOURCESMASK is a bitwise parameter that returns all possible causes of a drive disable. If a bit is set, the drive can be disabled for this reason.

The return value specific bits are as follows:

Bit Status and Response
0 Software triggered disable
1 Fault exists
2 Hardware Enable input inactive
3 In-rush relay state prevents enable
4 Initialization not complete
5 Controlled stop requested from digital input
6 Field bus requested disable

For most AKD models, this parameter will return the value 63.

General Information

Type

R/O parameter

Units

N/A

Range

N/A

Default Value

N/A

Data Type

Integer

Start Version

M_01-07-00-000

Related Topics

DRV.DISSOURCES

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen