DRV.DOWNLOADALLOWED

Description

This parameter returns whether the drive is in a safe state to begin a firmware download. A download can only be performed if the value is one. If the value is zero, WorkBench will block the download.

For an AKD or NSD, the value depends on the drive enable status. For a CPS, the value depends on the enable states of the NSDs on its string. If one more more NSDs are enabled on a string, download to the CPS will be blocked.

General Information

Type

R/O Parameter

Units

N/A

Range

0 to 1

Default Value

N/A

Data Type

Integer

Start Version

M_01-09-02-000

Related Topics

Limits

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen