DRV.MEMDATA
Description
DRV.MEMDATA reads or writes a value using the address set by DRV.MEMADDR . The write value accepts decimal or "0x" hexadecimal format. The read value defaults to decimal display but can be set to hexadecimal with the command "DRV.READFORMAT 16".
Examples
-
- These are example addresses. Never write to an address unless you are certain it is safe.
Read a value from internal address:
-->DRV.MEMADDR 0x1234.u32
--DRV.MEMDATA
3800219712
Write a decimal value to an internal address:
-->DRV.MEMDATA 123
Write a hexadecimal value to an internal address:
-->DRV.MEMDATA 0xFEDC
General Information
|
Type |
R/W Parameter |
|
Units |
N/A |
|
Range |
N/A |
|
Default Value |
N/A |
|
Data Type |
N/A |
|
Start Version |
M_01-00-00-000 |
|
Copyright © 2018 Kollmorgen |
|