DRV.NVCHECK
Description
DRV.NVCHECK returns a checksum of all the drives NV parameters. This parameter can be used to detect changes in parameters.
In some applications a master device needs to confirm the AKD drive contains an expected set of drive parameters. Reading and checking all the drive parameters individually is viable but this would be a long process involving many reads over the network. DRV.NVCHECK is a checksum on all the NV parameters and this parameter can be read in a single transaction. DRV.NVCHECK will return the same number if all the drive parameters match. If any of the drive parameters are changed then DRV.NVCHECK will return a different value.
General Information
|
Type |
R/O Parameter |
|
Units |
None |
|
Range |
N/A |
|
Default Value |
N/A |
|
Data Type |
Integer |
|
Start Version |
M_01-04-12-000 |
| Fieldbus |
Index/Subindex | Object Start Version |
|---|---|---|
| 3895h/0 | M_01-04-12-000 |
Related Topics
|
Copyright © 2018 Kollmorgen |
|