DRV.NVSAVE

Description

DRV.NVSAVE saves the current drive parameter values from the RAM to the NV memory.

The drive parameters that were saved to the NV are read from the NV on the next drive boot, causing the values to be automatically set to the saved values on every drive boot.

Executing DRV.RSTVAR does not modify the values of the NV, but instead sets the drive values in RAM to their defaults.

General Information

Type

Command

Units

N/A

Range

N/A

Default Value

N/A

Data Type

N/A

Start Version

M_01-00-00-000

FieldbusClosedA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design

Index/Subindex

Object Start Version

EtherCATClosedEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen

35EBh/0

M_01-00-00-000

*For Profinet, write a value of 0 into the PNU to execute a command.

Related Topics

DRV.RSTVAR

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen