DRV.PWD (Password Protected)

Description

DRV.PWD accesses the password-protected level of the drive.

For advanced users, additional password -protected commands and parameters are available. Improper use of these additional commands can cause permanent damage to the drive and void the drive warranty. Contact technical support for guidance on how to access and properly use these parameters and commands.

General Information

Type

Command

Units

N/A

Range

N/A

Default Value

N/A

Data Type

String

See Also

N/A

Start Version

M_01-00-00-000

SynqNetClosedSynqNet is a digital machine control network. Built on the 100BT physical layer, SynqNet provides a synchronous real-time connection between motion controllers, servo drives, stepper drives, I/O modules, and custom devices Information
Range 0

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen