DRV.TIME
Description
A continuous time counter in the drive. The timer starts at zero and counts up until it rolls over. If a new value is written to the timer, it continues to count up starting at the written value. The DRV.TIME value is set to zero when the AKD BASIC is powered on.
General Information
|
Type |
R/W |
|
Units |
Milliseconds |
|
Range |
0 to 4294967295 (~ 49 days) |
|
Default Value |
N/A |
|
Data Type |
Integer |
|
Start Version |
|
Related Topics
DRV.RUNTIME | WHEN.DRV.TIME
|
Copyright © 2018 Kollmorgen |
|