ECAT.LEGACYREV

Description

The ECAT.LEGACYREV defines the revision number located in the EtherCATClosedEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs slave information (EEprom).

Value Description
0 Revision number is set to actual revision (e.g. for FW 1.16 #x00160000). Note: The revision number will change with for next releases.
1 Revision number is set to legacy value of #x00000002.

General Information

Type

NV Parameter

Units

N/A

Range

0 to 1

Default Value

1

Data Type

Integer

Start Version

M_01-16-00-001

FieldbusClosedA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design Index/Subindex Object Start Version

EtherCAT COE and CANopen

541Dh/1 M_01-16-00-001

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen