FBUS.SYNCWND

Description

This parameter sets symmetrically arranged window around the desired sync distance.

General Information

Type

NV Parameter

Units

ns

Range

0 to 1,000,000 ns

Default Value

50,000 ns

Data Type

Integer,  U2

See Also

Appendix B: FieldbusClosedA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design Manuals

Start Version

M_01-00-00-000

Fieldbus

Index/Subindex

Object Start Version

EtherCATClosedEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen

3496h/3

M_01-00-00-000

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen