HWLS.NEGSTATE

Description

HWLS.NEGSTATE reads the status of the negative HW limit switch as follows:

0 = Low

1 = High

General Information

Type

R/O Parameter

Units

0 to 1

Range

N/A

Default Value

Integer

Data Type

HWLS.POSSTATE

See Also

N/A

Start Version

M_01-00-00-000

Related Topics

 

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen