IL.CMDU

Description

This parameter sets the user current command value.

The current command value, which is provided to the current loop (ILClosed"Instruction list" This is a low-level language and resembles assembly.CMD), can be limited further using a parameter setting or I2t calculation. IL.CMDU is limited also by motor peak current, IL.LIMITN and IL.LIMITP .

For IPM motors (MOTOR.TYPE = 6), IL.CMDU is decomposed into d-component and q-component current values, as both are used for closed loop current control. The d-component value is used to set IL.DCMD, and the q-component value is used to set IL.CMD .

General Information

Type

R/W Parameter

Units

Arms

Range

Minimum range value = maximum of IL.LIMITN and -MOTOR.IPEAK

Maximum range value = minimum of IL.LIMITP and MOTOR.IPEAK

Default Value

0 Arms

Data Type

Float

See Also

DRV.IPEAK , DRV.OPMODE ,DRV.CMDSOURCE

Start Version

M_01-00-00-000

Related Topics

1    Current Loop

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen