IL.DEADBAND (Password Protected)
Description
This parameter displays the dead time between two IGBTs in series connection. The dead time depends on the type of power board.
General Information
|
Type |
R/O Parameter |
|
Units |
ns |
|
Range |
N/A |
|
Default Value |
N/A |
|
Data Type |
Integer |
|
See Also |
N/A |
|
Start Version |
M_01-00-00-000 |
|
Copyright © 2018 Kollmorgen |
|