IL.DIFOLD

Description

ILClosed"Instruction list" This is a low-level language and resembles assembly.DIFOLD is the output of the drive foldback algorithm. It is an artificial current, which can be higher or lower than the drive peak current (DRV.IPEAK). When IL.DIFOLD is lower than the existing current limit (such as IL.LIMITP ), it becomes the active current limit.

IL.DIFOLD decreases when the actual current is higher than drive continuous current and increases (up to a certain level) when the actual current is lower than drive continuous current.

General Information

Type

R/O Parameter

Units

Arms

Range

0 to 2,147,483.647 Arms

Default Value

N/A

Data Type

Float

See Also

Foldback

Start Version

M_01-00-00-000

FieldbusClosedA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design

Index/Subindex

Object Start Version

EtherCATClosedEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen

3559h/0

M_01-00-00-000

Related Topics

1    Current Loop

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen