IL.FBSOURCE

Description

This parameter selects the feedback source that current loop uses for commutation angle calculation. It applies only when MOTOR.TYPE = 4.

0 = Primary feedback

1 = Secondary feedback

2 = Tertiary feedback

When ILClosed"Instruction list" This is a low-level language and resembles assembly.FBSOURCE is changed, MOTOR.POLES and MOTOR.PHASE are updated.

IL.FBSOURCE MOTOR.PHASE is set to: MOTOR.POLES is set to:
0 FB1.MOTORPHASE FB1.MOTORPOLES
1 FB2.MOTORPHASE FB2.MOTORPOLES
2 FB3.MOTORPHASE FB3.MOTORPOLES

For induction motor closed loop control the commutation angle is set as shown in the following figure.

General Information

Type

R/W

Units

N/A

Range

0 to 2

Default Value

0

Data Type

Integer

Start Version

M_01-08-00-000

FieldbusClosedA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design

Index/Subindex

Object Start Version

EtherCATClosedEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen

5361h/0

M_01-08-00-000

Related Topics

MOTOR.TYPE

FB1.MOTORPOLES | FB2.MOTORPOLES | FB3.MOTORPOLES

FB1.MOTORPHASE | FB2.MOTORPHASE | FB3.MOTORPHASE

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen