IL.MFOLDD

Description

ILClosed"Instruction list" This is a low-level language and resembles assembly.MFOLDD sets the maximum time allowed for the motor to remain at peak current before starting to fold towards the motor continuous current. When at motor peak current, IL.MFOLDD is the amount of time before the foldback algorithm starts to reduce the current.

General Information

Type

R/O Parameter

Units

s

Range

0.1 to 2400 s

Default Value

10 s

Data Type

Float

See Also

Foldback

Start Version

M_01-00-00-000

Related Topics

1    Current Loop

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen