IL.MFOLDR

Description

ILClosed"Instruction list" This is a low-level language and resembles assembly.MFOLDR sets the recovery time for the motor foldback algorithm. If 0 current is applied for at least the recovery time duration, it is possible to apply motor peak current for the duration of IL.MFOLDD time.

The IL.MFOLDR value is automatically calculated from other foldback parameters.

General Information

Type

R/O Parameter

Units

s

Range

0.1 to 65,535 s

Default Value

Calculated from other foldback parameters.

Data Type

Float

See Also

Foldback

Start Version

M_01-00-00-000

Related Topics

1    Current Loop

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen