IL.MIMODE

Description

This parameter determines the method of the motor protection.

0 – The motor foldback mechanism is responsible for protecting the motor from overload.

1 – The Motor I2t algorithm is responsible for protecting the motor from overload.

General Information

Type

NV parameter

Units

N/A

Range

0 to 1

Default Value

0

Data Type

Integer

See Also

IL.MI2T,  IL.MI2TWTHRESH

Start Version

M_01-04-01-000

FieldbusClosedA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design

Index/Subindex

Object Start Version

EtherCATClosedEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen

3427h/1

M_01-00-00-000

Related Topics

Foldback

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen