IL.VCMD

Description

Reads the output of the current loop that controls the q-component of the current.

General Information

Type

R/O Parameter

Units

VrmsClosedrms stands for root mean square (also known as the quadratic mean)

Range

0 Vrms to bus voltage

Default Value

N/A

Data Type

Integer

Start Version

M_01-00-00-000

Related Topics

1    Current Loop

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen