MOTOR.BRAKESTATE

Description

This parameter reads the actual status of the motor brake and can only show two states:

1 = Brake released or not present

2 = Brake applied

General Information

Type

R/O Parameter

Units

N/A

Range

Brake released or not present.

Brake applied.

Default Value

Brake applied or not present.

Data Type

String

See Also

N/A

Start Version

M_01-00-00-000

Related Topics

Motor

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen