MOTOR.IDDATAVALID

Description

MOTOR.IDDATAVALID reports the status of the motor memory status.

The valid values for this keyword are the following:

Value

Description

0

Error in identification

1

Success in identification

2

Identification in process

3

Identification not started yet

4

Success recognizing feedback, but failed to varify OEMClosed"Original equipment manufacturer" A term that refers to containment-based re-branding, namely where one company uses a component of another company within its product, or sells the product of another company under its own brand. OEM refers to the company that originally manufactured the product data integrity

General Information

Type

R/O Parameter

Units

N/A

Range

N/A

Default Value

0

Data Type

Integer

See Also

N/A

Start Version

M_01-02-00-000

Related Topics

Motor

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen