MOTOR.IDMAX
Description
This parameter is supported for IPM motors (MOTOR.TYPE = 6). MOTOR.IDMAX is the maximum motor winding current in the direct (non-torque
Torque is the tendency of a force to rotate an object about an axis. Just as a force is a push or a pull, a torque can be thought of as a twist producing) axis.
-
-
This parameter is automatically configured for (Undefined variable: MyVariables.CompanyName) motors when MOTOR.AUTOSET = 1.
General Information
|
Type |
NV Parameter |
|
Units |
Arms |
|
Range |
0.2 to 1000 |
|
Default Value |
0.5 * MOTOR.IPEAK |
|
Data Type |
Float |
|
Start Version |
M_01-11-00-000 |
Related Topics
|
Copyright © 2018 Kollmorgen |
|