MOTOR.IMID

Description

The value of ILClosed"Instruction list" This is a low-level language and resembles assembly.IMID can be estimated using the motor name plate information.

The following rule should generally be used:

In which Id is the value for IL.IMID, the preset rotor flux building current, Ir is the name plate phase current, cosϕ is the name plate power factor at rated and operation, and 0.8 is an empirical factor (accounts for the angle error due to voltage drop on the leakage induction).

General Information

Type

R/W

Units

Arms

Range

0 to DRIVE.IPEAK

Default Value

0

Data Type

Float

Start Version

M_01-08-00-000

FieldbusClosedA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design

Index/Subindex

Object Start Version

EtherCATClosedEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen

5362h/0

M_01-08-00-000

Related Topics

Motor

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen