MOTOR.INERTIA
Description
This parameter sets the motor inertia.
-
-
This parameter is automatically configured for (Undefined variable: MyVariables.CompanyName) motors when MOTOR.AUTOSET=1.
General Information
|
Type |
NV Parameter |
|
Units |
kgcm² for rotary motors kg for linear motors |
|
Range |
1 to 200,000 kgcm² or kg |
|
Default Value |
100 kgcm² or kg |
|
Data Type |
Float |
|
See Also |
N/A |
|
Start Version |
M_01-00-00-000 |
|
Index/Subindex |
Object Start Version |
|
|---|---|---|
|
35ABh/0 |
M_01-00-00-000 |
Related Topics
|
Copyright © 2018 Kollmorgen |
|