MOTOR.LQLL
Description
This parameter is used to configure the motor line-to-line inductance.
-
-
This parameter is automatically configured for (Undefined variable: MyVariables.CompanyName) motors when MOTOR.AUTOSET=1.
General Information
|
Type |
NV Parameter |
|
Units |
mH |
|
Range |
1 to 232 mH |
|
Default Value |
17.000 mH |
|
Data Type |
Float |
|
See Also |
N/A |
|
Start Version |
M_01-00-00-000 |
|
Index/Subindex |
Object Start Version |
|
|---|---|---|
|
3455h/0 |
M_01-00-00-000 |
Related Topics
|
Copyright © 2018 Kollmorgen |
|