MOTOR.NAME

Description

This parameter is used to set the motor name.


  • This parameter is automatically configured for (Undefined variable: MyVariables.CompanyName) motors when MOTOR.AUTOSET=1.

General Information

Type

NV Parameter

Units

N/A

Range

11 chars

Default Value

N/A

Data Type

String

See Also

N/A

Start Version

M_01-00-00-000

Related Topics

Motor

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen