MOTOR.R

Description

MOTOR.R sets the stator winding resistance phase-to-phase in ohms.


  • This parameter is automatically configured for (Undefined variable: MyVariables.CompanyName) motors when MOTOR.AUTOSET=1.

General Information

Type

NV Parameter

Units

Ω

Range

0.001 to 650 Ω

Default Value

10 Ω

Data Type

Float

See Also

N/A

Start Version

M_01-00-00-000

FieldbusClosedA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design

Index/Subindex

Object Start Version

EtherCATClosedEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen

3456h/0

M_01-00-00-000

Related Topics

Motor

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen