MOTOR.RTYPE
Description
This parameter defines the type of thermal resistor used inside of the motor to measures motor temperature.
For firmware versions prior to 01-10-02-000, parameter range is 0 to 1.
0 = PTC
1 = NTC
For firmware versions 01-10-02-000 and later, parameter range is 0 to 255.
0 = Single PTC Thermistor
1 = Single NTC Thermistor
2 = KTY83-110 Thermistor
3 = KTY84-130 Thermistor
4 = PTC + KTY83-110 Thermistors
5 = Thermal switch
255 = No thermal sensor
A sensor is a type of transducer that converts one type of energy into another for various purposes including measurement or information transfer in the motor
-
-
For firmware versions 01-09-00-000 and later, this parameter is automatically configured for (Undefined variable: MyVariables.CompanyName) motors when MOTOR.AUTOSET = 1.
General Information
|
Type |
NV Parameter |
|
Units |
N/A |
|
Range |
0 to 1 For firmware version 01-10-02-000 and later, range is 0 to 255. |
|
Default Value |
0 |
|
Data Type |
Integer |
|
Start Version |
M_01-00-00-000 |
|
Index/Subindex |
Object Start Version |
|
|---|---|---|
|
50FEh/0 |
M_01-00-00-000 |
Related Topics
|
Copyright © 2018 Kollmorgen |
|