MOTOR.SUPPORTEDPARAMS
Description
This parameter lists all the MOTOR parameters that are supported for the motor type selected by the MOTOR.TYPE parameter.
Example
The following output is produced for surface permanent magnet motors (MOTOR.TYPE = 0).
--> MOTOR.SUPPORTEDPARAMS
MOTOR.CTF0
MOTOR.ICONT
MOTOR.INERTIA
MOTOR.IPEAK
MOTOR.KE
MOTOR.KT
MOTOR.LISAT
MOTOR.LQLL
MOTOR.PHASE
MOTOR.POLES
MOTOR.R
MOTOR.VMAX
MOTOR.VOLTMAX
General Information
|
Type |
R/O Parameter |
|
Units |
N/A |
|
Range |
N/A |
|
Default Value |
N/A |
|
Data Type |
String |
|
Start Version |
M_01-11-00-000 |
Related Topics
|
Copyright © 2018 Kollmorgen |
|