PL.GEARIN
Description
PL.GEARIN sets the gear factor for the position loop output values towards the velocity loop input values. PL.GEARIN is the numerator of the gear factor. PL.GEAROUT describes the denominator of the gear factor.
This gear factor is useful in applications where the position loop is closed by an external encoder (PL.FBSOURCE != 0) and the velocity loop is closed by the motor feedback encoder (VL.FBSOURCE = 0). If there is a mechanical gear factor between the external encoder and the motor feedback encoder, PL.GEARIN and PL.GEAROUT are used to described this physical gearing. Setting of the gear factor is important to achieve a high performance tuning result for the axis.
General Information
|
Type |
NV Parameter |
|
Units |
N/A |
|
Range |
1 to 8192 |
|
Default Value |
1 |
|
Data Type |
Integer |
|
Start Version |
M_01-16-08-001 |
Related Topics
Position Loop
|
Copyright © 2018 Kollmorgen |
|