REC.RETRIEVESIZE

Description

This parameter sets the number of samples that REC.RETRIEVEDATA returns.

WorkBench also uses this parameter to set the number of samples returned when retrieving the data continuously for RT recoding.

Use REC.RETRIEVE for the complete recording information view.

General Information

Type

R/W Parameter

Units

recorder samples

Range

0 to 65,535 recorder samples

Default Value

1,000 recorder samples

Data Type

Integer

See Also

REC.RETRIEVEDATA, REC.RETRIEVEHDR

Start Version

M_01-00-00-000

Related Topics

Scope

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen