REC.STOPTYPE
Description
This parameter sets the stop type for the recording.
0 = Recorder fills in the buffer once.
1 = Recorder runs, continuously filling the recording circular buffer.
To stop RT recording, execute REC.OFF.
General Information
|
Type |
R/W Parameter |
|
Units |
N/A |
|
Range |
0 or 1 |
|
Default Value |
0 |
|
Data Type |
Integer |
|
See Also |
REC.RETRIEVEDATA, REC.RETRIEVESIZE |
|
Start Version |
M_01-00-00-000 |
Related Topics
|
Copyright © 2018 Kollmorgen |
|