REC.TRIG
Description
REC.TRIG starts the trigger according to the trigger type defined by REC.TRIGTYPE.
REC.TRIG sets the value of REC.DONE to 0.
After calling REC.TRIG, the data that was recorded by previous recording is deleted and cannot be retrieved.
No REC parameters can be set after a call to REC.TRIG until the recorder has finished or until REC.OFF is executed.
General Information
|
Type |
Command |
|
Units |
N/A |
|
Range |
N/A |
|
Default Value |
N/A |
|
Data Type |
N/A |
|
See Also |
REC.RETRIEVE, REC.OFF |
|
Start Version |
M_01-00-00-000 |
*For Profinet, write a value of 0 into the PNU to execute a command.
Related Topics
|
Copyright © 2018 Kollmorgen |
|