REC.TRIGSLOPE

Description

REC.TRIGSLOPE sets the recorder trigger slope. This parameter is only used when REC.TRIGTYPE = 2 or 3.

General Information

Type

R/W Parameter

Units

0 = Negative

1 = Positive

Range

0 to 1

Default Value

0

Data Type

Integer

See Also

REC.TRIG, REC.NUMPOINTS

Start Version

M_01-00-00-000

Related Topics

Scope

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen