STO.STATE
Description
STO.STATE returns the status of the safe torque
Torque is the tendency of a force to rotate an object about an axis. Just as a force is a push or a pull, a torque can be thought of as a twist off.
AKD003 up to AKD024 (one STO channel)
| Value | Description |
|---|---|
| 1 | Safe torque on (no STO fault/warning) |
| 0 | Safe torque off (STO fault and warning are present) |
1 - Safe torque on (no safe torque off fault/warning).
0 - Safe torque off (safe torque off fault/warning).
When STO.STATE = 1, the drive can be enabled.
AKD048 (two STO channels)
An STO fault and warning are generated when either STO1 or STO2 are not on. Use STO.STATE to determine the source (STO1 or STO2) of the STO fault. WorkBench also displays the status of both STO1 and STO2 at the bottom of the screen.
| Value | Description |
|---|---|
| 3 | STO1 and STO2 are on (no STO fault/warning) |
| 2 | STO1 is off, and STO2 is on (STO fault and warning are present) |
| 1 | STO1 is on, and STO2 is off (STO fault and warning are present) |
| 0 | STO1 and STO2 are off (STO fault and warning are present) |
General Information
|
Type |
R/O Parameter |
|
Units |
N/A |
|
Range |
0 to 1 for drives with only one STO (AKD003 up to AKD024) 0 to 3 for drives that support STO2 (AKD048 ) |
|
Default Value |
N/A |
|
Data Type |
Integer |
|
See Also |
N/A |
|
Start Version |
M_01-00-00-000 |
Related Topics
Safe Torque
Torque is the tendency of a force to rotate an object about an axis. Just as a force is a push or a pull, a torque can be thought of as a twist Off (STO) (➜ p. 1)
|
Copyright © 2018 Kollmorgen |
|