SWLS.STATE

Description

This parameter reads the status word of the software limit switches. The status word indicates the result of the compare between the software limit switch compare register and the actual position of the position loop.

Example

Bit 0 = 0: SWLS.LIMIT0 is not active.

Bit 0 = 1: SWLS.LIMIT0 is active.

Bit 1 = 0: SWLS.LIMIT1 is not active.

Bit 1 = 1: SWLS.LIMIT1 is active.

Bits 2 to 7 are currently not in use.

General Information

Type

R/O Parameter

Units

N/A

Range

0 to 3

Default Value

0

Data Type

U8

Start Version

M_01-00-00-000

Related Topics

Limits

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen