TEMP.POWER1 to TEMP.POWER3

Description

Reads the temperature of the power board(s) temperature sensorClosedA sensor is a type of transducer that converts one type of energy into another for various purposes including measurement or information transfer(s). Most AKDs have only one power board sensor which is read by TEMP.POWER1.

General Information

Type

R/O Parameter

Units

Degrees Celsius

Range

-127 to 128

Default Value

N/A

Data Type

Integer

Start Version

M_01-09-00-000

Related Topics

DRV.TEMPERATURES | TEMP.CONTROL

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen