VBUS.OVWTHRESH
Description
If VBUS.VALUE value exceeds VBUS.OVWTHRESH, then a warning is generated. The warning is removed if the voltage returns to below 97% (1/32) of the overvoltage warning level.
General Information
|
Type |
NV Parameter |
|
Units |
VDC |
|
Range |
0 to 900 VDC |
|
Default Value |
0 VDC (warning disabled) |
|
Data Type |
U16 |
|
See Also |
N/A |
|
Start Version |
M_01-00-00-000 |
|
Index/Subindex |
Object Start Version |
|
|---|---|---|
|
518Eh/0 |
M_01-00-00-000 |
Related Topics
|
Copyright © 2018 Kollmorgen |
|