VL.ARTYPE1 TO VL.ARTYPE4
Description
These parameters indicate the method used to calculate the biquad coefficients VL.ARPFx, VL.ARPQx, VL.ARZFx, and VL.ARZQx. A value of 0 indicates that the coefficients are set directly. This parameter has no effect on the filter itself, but is only used to determine the original design parameters. Currently, only the value of 0 is supported.
General Information
|
Type |
NV Parameter |
|
Units |
N/A |
|
Range |
0 |
|
Default Value |
0 |
|
Data Type |
U8 |
|
See Also |
N/A |
|
Start Version |
M_01-00-00-000 |
| Fieldbus |
Index/Subindex | Object Start Version | |
|---|---|---|---|
|
3405h/1 |
M_01-02-00-000 | ||
|
3405h/2 |
|||
|
3405h/3 |
|||
|
3405h/4 |
|||
Related Topics
1 Velocity Loop
|
Copyright © 2018 Kollmorgen |
|