VL.FB
Description
VL.FB returns the velocity feedback as it is received in the velocity loop, after passing through Filter 3 and Filter 4.
General Information
|
Type |
R/O Parameter |
|
Units |
Depends on UNIT.VROTARY (pg 1) or UNIT.VLINEAR (pg 1) Rotary: rpm, rps, deg/s, (custom units)/s, rad/s Linear: counts/s, mm/s, µm/s, (custom units)/s |
|
Range |
N/A |
|
Default Value |
N/A |
|
Data Type |
Float |
|
See Also |
|
|
Start Version |
M_01-00-00-000 |
|
Index/Subindex |
Object Start Version |
|
|---|---|---|
|
3618h/0 606Ch/0 |
M_01-00-00-000 |
Related Topics
Velocity Loop
|
Copyright © 2018 Kollmorgen |
|