WS.STATE

Description

WS switches different current vectors and records position feedback in order to establish commutation alignment.

WS.STATE 0 = wake and shake successful (DONE).

WS.STATE 1 = wake and shake configured and will be done at next enable (ARMED).

WS.STATE 2 = wake and shake running. (ACTIVE)

WS.STATE 10 = error occurred during wake and shake (ERROR).

WS.STATE 11 = wake and shake not required (IDLE).

General Information

Type

R/O Parameter

Units

N/A

Range

N/A

Default Value

Only valid before the first enable occurs.

11 - for feedback types that do not require wake and shake

1 - for feedback types that require wake and shake

Data Type

U8

See Also

N/A

Start Version

M_01-01-00-101, M_01-02-00-000

FieldbusClosedA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design

Index/Subindex

Object Start Version

EtherCATClosedEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen

3494h/5

M_01-00-00-000

Related Topics

Wake and Shake Overview

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen