COUNTOFPLCopen motion icon

FunctionClosedA function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. - Returns the number of items in an array

Inputs

ARR : ANY  Declared array

Outputs

Q : DINT   Total number of items in the array

Remarks

The input must be an array and can have any data type. This function is particularly useful to avoid writing directly the actual size of an array in a program, and thus keep the program independent from the declaration. Example:

   FOR i := 1 TO CountOf (MyArray) DO
      MyArray[i-1] := 0;
   END_FOR;

In FFLD language, the operation is executed only if the input rung (EN) is TRUE. The output rung (ENO) keeps the same value as the input rung.

Examples

array return
Arr1 [ 0..9 ] 10
Arr2 [ 0..4 , 0..9 ] 50

ST Language

Q := CountOf (ARR);

FBD Language

FFLD Language

(* The function is executed only if EN is TRUE *)
(* ENO keeps the same value as EN *)

IL Language

Not available

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen