INC
A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. - Increase a numerical variable
Inputs
IN : ANY Numerical variable (increased after call). Data In/Out
Outputs
Q : ANY Increased value
Remarks
When the function is called, the variable connected to the "IN" input is increased and copied to Q. All data types are supported except BOOL and STRING: for these types, the output is the copy of IN.
For real values, variable is increased by "1.0". For time values, variable is increased by 1 ms.
The IN input must be directly connected to a variable, and cannot be a constant or complex expression.
This function is particularly designed for ST
"Structured text"
A high-level language that is block structured and syntactically resembles Pascal language. It allows simplified
writing as assigning the result of the function is not mandatory.
ST Language
IN := 1;
Q := INC (IN);
(* now: IN = 2 ; Q = 2 *)
INC (IN); (* simplified call *)
FBD Language
FFLD Language
IL Language
not available
|
Copyright © 2018 Kollmorgen |
|