How to resolve errors
Device is not found
- Check if device is switched on
- Check the network connection
- Ensure the correct name was set on the device
Error setting the IP configuration
- Ensure that the IP configuration is valid and appropriate for your network
- Ensure the VLAN
"Virtual LAN"
A VLAN is a group of hosts with a common set of requirements that communicate as if they were attached to the Broadcast domain, regardless of their physical location. A VLAN has the same attributes as a physical LAN, but it allows for end stations to be grouped together even if they are not located on the same network switch. Network reconfiguration can be performed using software instead of physically relocating devices ID is setup correctly in the device settings
CL-RPC Lookup
Timeout error
- Ensure that the IP configuration is valid and appropriate for your network
- Increase the IP configuration delay
Other errors
- Ensure you use the correct device name
- Ensure you have chosen the correct GSDML file (also check if the GSDML file version is appropriate for the firmware version of the device)
Connect response error
Timeout error
- Ensure that the IP configuration is valid and appropriate for your network
- Increase the IP configuration delay
Connect response error
Depending on the PNIO status error check, if the settings listed in the table below are set appropriate for your device.
| PNIO Status | Check the specified setting |
|---|---|
| 1C010003 | Slave\ObjectUUID (correct GDML file) |
| DB81010A | Master\Activity timeout factor |
| DB81010B | Master\Controller name |
| DB81010C | Master\Controller name |
| DB810207 | Master\RT-Class |
| DB81020A | Master\Send clock factor |
| DB81020B | Slave\Reduction ratio |
| DB81020C | Slave\Phase |
| DB81020F | Master\Watchdog factor |
| DB810210 | Master\Watchdog factor |
| DB8103,* | Slave\Module IDs,IOs |
| DB810407 | Master\Alarm timeout |
| DB810408 | Master\Alarm retries |
Table 8-18: PNIO status error codes on connect and the related settings in the configuration
Module configuration is different
- Ensure you have configured the modules present on the device (If you have read the module configuration from the device, ensure you have selected the correct modules in the resolve ambiguous modules dialog displayed after selecting the GSDML file).
- Ensure you have chosen the correct GSDML file (also check if the GSDML file version is appropriate for the firmware version of the device).
Writing parameterization error (with status 0XDF80*)
- Ensure you have configured the modules present on the device (If you have read the module configuration from the device, ensure you have selected the correct modules in the resolve ambiguous modules dialog displayed after selecting the GSDML file).
- Ensure you have chosen the correct GSDML file (also check if the GSDML file version is appropriate for the firmware version of the device).
If your error could not be resolved using the hints above, update the firmware of your device and the GSDML file to the latest version and try again.
For further analyses record the PNIO communication using Wireshark.
- Start Wireshark and select Capture\Options from the menu.
- Choose the network interface used for the PNIO communication and enter the Capture filter below:
ether proto 0x8892 or (ether proto 0x8100 and ether[16:2]=0x8892) or udp port 0x8894
- Then click start.
- Start the runtime
In computer science, runtime (or run-time) describes the operation of a computer program, the duration of its execution, from beginning to termination (compare compile time).
Within KAS, runtime also refers to the virtual machine that manage the program written in a computer language while it is running with your application several times and then stop the Wireshark capturing by selecting Capture\Stop from the menu. You can save your recorded traffic by selecting File\Save from the menu.
|
Copyright © 2018 Kollmorgen |
|