ANY_TO_STRING
Inputs
IN : ANY Input value
Outputs
Q : STRING Value converted to string
Remarks
For BOOL input data types, the output is '1' or '0' for TRUE and FALSE
respectively. For DINT, REAL or TIME
input data types, the output is the string representation of the input number.
It is a number of milliseconds for TIME inputs. In FFLD
language, the conversion is executed only if the input rung (EN) is TRUE. The output rung
(ENO) keeps the same value as the input rung. In IL
"Instruction list"
This is a low-level language and resembles assembly language, the ANY_TO_STRING function
converts the current result.
ST Language
Q := ANY_TO_STRING (IN);
FBD Language
FFLD Language
(* The conversion is executed only if EN is TRUE *)
(* ENO keeps the same value as EN *)
IL Language:
Op1: FFLD IN
ANY_TO_STRING
ST Q
See also
ANY_TO_BOOL ANY_TO_SINT ANY_TO_INT ANY_TO_DINT ANY_TO_LINT ANY_TO_REAL ANY_TO_LREAL ANY_TO_TIME
|
Copyright © 2018 Kollmorgen |
|